Technical FAQs

Ask a Question

What is the terminal lug data for a SU2040M150R Combination Service Entrance Device?

The main phase and neutral lugs accept a #6 AWG - 250 KCMIL copper or aluminum conductor. The service ground lug accepts a #14 - #4 AWG copper or a #12 - #2 AWG aluminum conductor.


CTA-ID : 2032951
Was this helpful?
What can we do to improve the information ?