Technical FAQs

Ask a Question

Will the coil on a 8501KP12V24 operate at 208 volts AC?

Yes. The coil will operate between +10% to -15% of nominal voltage.


CTA-ID : 2032582
Was this helpful?
What can we do to improve the information ?