Technical FAQs

Ask a Question

Can you lock the D10S1 switch in the ``ON`` and ``OFF`` positions?<br />

Yes. The handle as shipped permits locking the switch in the ``OFF`` position. Locking the handle in the ON position requires the customer to `enable` the provision for locking the handle in the ``ON`` position. The material covering the locking notch on the handle plate must be removed with a hacksaw and/or file. In the ``ON`` position, the handle has a defeatable interlock. To defeat the interlock, use a screw driver to turn a slotted screw which will release the handle.



CTA-ID : 2032961
Was this helpful?
What can we do to improve the information ?