Technical FAQs

Ask a Question

Customer needed help wiring to the load terminals of a PGA36120

Refer to circuit breaker instruction manual. Send the T- handle 5/16`` allen wrench through the hollow top wire binding screw, into the bottom wire binding screws, tighten the wires closest to the back pan first. Then back the allen wrench out, unscrewing the top screw. Put the top wire in and tighten the top screw.


CTA-ID : 2033239
Was this helpful?
What can we do to improve the information ?