Technical FAQs

Ask a Question

Can the LA9CA* Insta kits be used for both NEMA 1 and NEMA 12 Enclosed IEC Starters?

Yes, all Insta kits are rated for use in NEMA 1 or NEMA 12 Enclosed IEC Starters.


CTA-ID : 2033222
Was this helpful?
What can we do to improve the information ?