Technical FAQs

Ask a Question

Which lug is the load neutral lug on the HOMELINE 2p GFI breaker?

The neutral is the one identified on the circuit breaker markings as the load neutral.  See instruction bulletin for more information.


CTA-ID : 2033217
Was this helpful?
What can we do to improve the information ?