Technical FAQs

Ask a Question

What are the repair parts for a SMS323TWR, Series E1 (E01)?

Issue:
What are the repair parts for a SMS323TWR, Series E1 (E01)?

Product Line:
Switches

Environment:
SMS Specialty QMB type switch

Cause:
repair parts required

Resolution:
The SMS device is a twin switch, meaning it contains two switches in the one device. Parts are listed per switch. Only the parts listed below are considered field replaceable:
Arc Shield/Suppressor Assembly (1 required) - 4051239950
Load Base Assembly (1 required, includes lugs) - 4052068050
Load Base Mounting Screw (2 required per load base) - 4020506501
Handle Knob Kit - 4028343750

 


 
Was this helpful?
What can we do to improve the information ?