Technical FAQs

Ask a Question

Can the QO20L125, Series G1 load center be converted to a main breaker load center?

Issue:
Product feature

Product Line:
Obsoleter QO LC

Cause:
Convert MLO to MB

Resolution:
A QOM1-VH main circuit breaker kit can be used in the QO20L125, Series G1 main lugs load center to convert it to a main circuit breaker load center, up to 125A maximum. 
To convert to main breaker, order:
50A = QOM50VH
60A = QOM60VH
70A = QOM70VH
80A = QOM80VH
90A = QOM90VH
100A = QOM100VH
110A = QOM110VH
125A = QOM125VH


CTA-ID : 2033221
Was this helpful?
What can we do to improve the information ?