Technical FAQs

Ask a Question

What is the Terminal Lug Data for a CD326N, Series E3 General Duty safety switch?

The lugs on this device will accept (2) #4 AWG - 600 kcmil copper or aluminum conductors per phase. However, wire bending space available in the switch restricts the conductors to (2) 500 kcmil maximum.


CTA-ID : 2033200
Was this helpful?
What can we do to improve the information ?