Technical FAQs

Ask a Question

Does the PCF breaker come with mounting feet like the PAF and PHF circuit breakers?

No. The PCF is supplied with terminal pads for line and load ends of the circuit breaker as standard. Mounting feet cannot be used with it and none are included.

CTA-ID : 2033042
Was this helpful?
What can we do to improve the information ?