Technical FAQs

Ask a Question

How can I get the two screws to mount a Kirk lock to the Powerpact P or R provision?

These screws should come in a small bag with the provision. Part number 48186-235-50 is available, but not profiled, from Missouri. Contact Customer Service in Cedar Rapids to obtain these screws.
You will need a special 7/32 allen wrench to install the protected allen head screws.


CTA-ID : 2032829
Was this helpful?
What can we do to improve the information ?