Technical FAQs

Ask a Question

What temperature range will the 9007C limit switches operate at?

Lever type -20 degrees F to 185 degree Fs
Plunger type 0 degrees to 185 degrees F


CTA-ID : 2032526
Was this helpful?
What can we do to improve the information ?