Technical FAQs

Ask a Question

Can you change the main disconnect in the SC2040M200F from 200 amp to 150 amp, in the field?

This device is UL listed for use with a main device up to 200 ampere maximum, so a 150 ampere main disconnect would be allowed. To convert the SC2040M200F to a 150 ampere device, remove the QOM2200VH factory installed main breaker and field install a QOM2150VH. The replaced QOM2200VH is not a returnable item.




CTA-ID : 2033075
Was this helpful?
What can we do to improve the information ?