Technical FAQs

Ask a Question

What is the part number for the cable for a XS8C1A1MAL01U20?<br /><br />

XSZCK111Y is the 2 meter straight connector cable; XSZCK101Y is the 2 meter 90 degree connector. Due to an error in the catalog, these cordsets do not follow the normal numbering convention. All cables described are also compatible with the older ``K`` suffix sensors.

CTA-ID : 2032859
Was this helpful?
What can we do to improve the information ?