Technical FAQs

Ask a Question

What is the tolerance or voltage range for NEMA starter coils?

NEMA specifications require the coils to operate at a range of -15% to +10%.


CTA-ID : 2032485
Was this helpful?
What can we do to improve the information ?