Technical FAQs

Ask a Question

What is the DC voltage rating for a QOU breaker?

It is 5 kA @ 48 Vdc for 1P and 2P, 10-70 A and 3P 10-60 A only.
QOU is UL Listed for 60 Vdc per pole 80-100 A, 1P; 80-125 A, 2P; and 70-100 A, 3P. AIR = 5 kA

CTA-ID : 2033150
Was this helpful?
What can we do to improve the information ?