Technical FAQs

Ask a Question

What is the part number for a separate mount NEMA size 1 overload relay?

The following outlines the overloads based on type desired:

Solid State Overload Relay:
Class 10 9065SS110
Class 20 9065SS120
Please note these overloads are intended for balanced three phase applications. Current range is adjustable from 9 to 27 amps, 600 vac maximum.

Melting Alloy:
Single pole contruction;
9065CO1 for left hand type
9065CO1R for right hand type
Three pole construction;
Please note that the melting alloy overloads are rated 25 amp 600 vac maximum.

Non-compensated 9065SEO6B2
Ambient temperature compensated 9065SEO6B
Please note that the bimetallic overload relays are rated 26 amp, 600 vac maximum.

CTA-ID : 2033152
Was this helpful?
What can we do to improve the information ?