Technical FAQs

Ask a Question

What is included in the QOCRBGK1 & HOMCRBGK1 Generator Interlock kit?

Product Features

Product Line:
QO and Homeline load centers

The Kits include drilling template for mounting kit & a retaining bracket to retain the branch circuit breaker to the Interior. It also includes a Interlock mechanism that Interlocks the QOM1, main circuit breaker with the QO or Homeline branch circuit breaker.

CTA-ID : 2033149
Was this helpful?
What can we do to improve the information ?