Technical FAQs

Ask a Question

What is a SDM38VHIR?

The SDM38VHIR is a Square D Multi-Link Structured Wiring component. It is an amplified Video Hub, for use with CATV or terrestrial antenna systems, used to distribute up to 3 video source signals to 8 TV outlets. One video source would be from the CATV or terrestrial antenna system and two video sources would be modulated input sources from peripherals such as a VCR, DVD or satellite antenna. A 120Vac power supply is included.

CTA-ID : 2032981
Was this helpful?
What can we do to improve the information ?