Technical FAQs

Ask a Question

What is a SDM1VWP?

The SDM1VWP is a wall plate that has RCA inputs on the front and Cat-5 outputs on the rear. It is used most commonly used in conjunction with Channel Injectors SDM11VMB or SDM11VMH. The Channel Injectors are supplied with Cat-5 inputs. Therefore, a SDM11VWP could be used to interface a video source with RCA outputs to the channel injectors.


CTA-ID : 2033135
Was this helpful?
What can we do to improve the information ?