Technical FAQs

Ask a Question

What are the repair parts for a QO11624L125GRB, Series S02?

Issue:
Current design repair parts

Product Line:
QO load centers

Environment:
Repair parts

Cause:
Maintenance

Resolution:
Only the parts listed below are considered field replaceable.
RB Cover - 4056317750
Interior Trim with Labels - 4056313001K
Interior Assembly - QO11624L125GRBI
Neutral Bonding screw - 4028345850K
Main Lugs - QOL125
Outdoor Cover latch - 4056314701
Latch Rivet - 2410212160
Interior trim mounting screw - 4020513001K
RB door mounting screws - 2142217101
Main circuit breaker and main lugs keps nut -2342702001


CTA-ID : 2033126
Was this helpful?
What can we do to improve the information ?