Technical FAQs

Ask a Question

What is the maximum current the contacts can handle on a XUC9ARCTL2 photo sensor?

Per page 102 of the 9006CT0101 catalog the maximum load on the contacts is 3 Amps. Bear in mind that this is RESISTIVE current. Any inductive load [relay coil, solenoid valve, etc.] will de-rate the contacts. It is always good practice to place an interposing relay in the circuit if the load is large or very inductive.


CTA-ID : 2033103
Was this helpful?
What can we do to improve the information ?