Technical FAQs

Ask a Question

Are the ABL Power Supplies UL Class 2 rated?

ABL7RM1202 and ABL7RM2401 are protection class conforming to VDE 01061: Class II without ground terminal (double insulated). There is no protection class for the ABL7RE devices.

CTA-ID : 2032886
Was this helpful?
What can we do to improve the information ?