Technical FAQs

Ask a Question

What is a SDM21VT?

The SDM21VT is a Square D Multi-Link Structured Wiring component. It is a set-top amplified modulator (it does not mount into the Multi-Link mounting bracket or enclosure). It will accept source baseband signals from a security camera, VCR. DVD or satellite antenna, via RCA video and audio inputs. Two sets of RCA inputs are provided for source signals. A single RG-6 coaxial cable output and two IR emitter outputs are provided. A 120Vac power supply is included.


CTA-ID : 2032985
Was this helpful?
What can we do to improve the information ?