Technical FAQs

Ask a Question

What is a SDM11VMH?

The SDM11VMH is a Square D Multi-Link Structured Wiring component. It injects a modulated input from a security camera, VCR, DVD or satellite antenna onto the RF signal from an omni-directional CATV or terrestrial antenna system. It is a single channel combination modulator, high headroom amplifier, and isolator. It is supplied with a Cat-5 input for the source to be modulated and a RG-6 coaxial cable input for the omni-directional CATV or terrestrial antenna signal. A 120Vac power supply is included.


CTA-ID : 2032983
Was this helpful?
What can we do to improve the information ?