Technical FAQs

Ask a Question

In the PX breaker with ground fault do you need the neutral CT for the ground fault trip to work?

A neutral sensor is required in 3ph 4 wire systems when the neutral wire is pulled and used for single phase loads. When a neutral is not pulled due to having all 3 phase loads, the NCT is not required.

CTA-ID : 2032085
Was this helpful?
What can we do to improve the information ?