Technical FAQs

Ask a Question

On horizontally mounted busway, can 100A busplugs be mounted in a vertical direction on it? Or, does the long dimension of the busplug run parallel with the bus?

The 100A busplugs can be mounted horizontally or vertically, but on a horizontal run, the long dimension of the busplug will hang downward from the busway. There is only one way to mount it.


CTA-ID : 2032069
Was this helpful?
What can we do to improve the information ?