Technical FAQs

Ask a Question

What torque is required on the jaw bolt of the FIB I-Line breaker?

Issue:
What torque is required on the jaw bolt of the FIB I-Line breaker?

Product Line:
I line panelboards or switchboards with I line distribution.

Environment:
Products sold in the United States.

Cause:
Product features, Installation

Resolution:
Use 20 inch-pounds of torque as stated in the Owners Manual #48049-033-02.


CTA-ID : 2032103

Was this helpful?
What can we do to improve the information ?