Technical FAQs

Ask a Question

What is the increase in capacity (kVA) of a liquid filled transformer with a 55/65 degree C temperature rise?

The increase in capacity (kVA) is 12% above the base kVA. The base kVA is the 65 degree C temperature rise.

CTA-ID : 2031980
Was this helpful?
What can we do to improve the information ?