Technical FAQs

Ask a Question

Can a HC4486WP weatherproof enclosure be secured to a wall, but with the base resting on the floor? Will the enclosure actually support the weight of the entire panelboard?

Issue:
Can a  HC4486WP weatherproof enclosure be secured to a wall, but with the base resting on the floor?  Will the enclosure actually support the weight of the  entire panelboard?

Product Line:
I Line panelboard

Environment:
Installation

Cause:
Mounting Clarification

Resolution:
Thes weatherproof enclosures can be free standing on base channels if ordered as a factory special. Because of this, the bottom of the can can actually support the weight of the entire panel, if the bottom endwall is resting on the floor.


CTA-ID : 2032042
Was this helpful?
What can we do to improve the information ?