Technical FAQs

Ask a Question

What is the overall length of a ZCKE08 ?<br />

It is 5.5`` from the bottom of the head to the top of the stick . There is no longer option available in the XCKJ family . If a longer length is required , consider a 9007C switch with a 9007JS** head .

CTA-ID : 2032024
Was this helpful?
What can we do to improve the information ?