Technical FAQs

Ask a Question

Will a QO2L30S accept a two pole QO breaker with an electrical accessory?

Yes, it will accept a two pole QO breaker with electrical accessory. It will not accept type EPD or GFI. The 30 amp load center rating should not be exceeded at 30 amp, or 25 amp, when Aluminum wire is used .


CTA-ID : 2032027
Was this helpful?
What can we do to improve the information ?