Technical FAQs

Ask a Question

What Class of fuse does the H327, H327N, H327R, H327NR, H327AWK and H327NAWK, heavy duty safety switches accept?

Issue:
Product design features

Product Line:
Heavy Duty Safety Switches

Environment:
Fuses

Cause:
Installation

Resolution:
These switches accept Class L fuses ONLY. With Class L fuses installed, the switches are UL listed for use on systems with up to 200,000 RMS Symmetrical Amperes available fault current.

NOTE: Class L is a 600V construction fuse that is used in these 240V rated switches.


CTA-ID : 2031851
Was this helpful?
What can we do to improve the information ?