Technical FAQs

Ask a Question

What is the maximum wire size control wire terminal the S37423 and S37424 will accept? This is for Powerpact H and J frame breakers.

What is the max wire size for control wire terminals for Powerpact H and J frames breakers?

Product Line:
Powerpact H and J frame

Products sold in North America

Need control wire on a Powerpact H or J frame.

Each control-wire terminal has a 1/4 in. (6.3mm) male spade connector tab which allows monitoring of circuit status.

Use catalog number S37423 for H frame, and S37424 for J frame.

See instruction bulletin, 48940-233-01

CTA-ID : 2031847
Was this helpful?
What can we do to improve the information ?