Technical FAQs

Ask a Question

Does Square D offer the QO load center covers painted 'White' instead of the standard gray cover?

Issue:
Product Design features

Product Line:
QO Load Centers

Environment:
Paint

Cause:
Application

Resolution:
Yes. Most of the QO load center covers are available in what is called an 'Appliance White' (this is basically a Semi-gloss finish white). For a catalog number just add the suffix 'W' to the standard cover catalog number, for example QOC16UF'W' or QOC16US'W'. All the available white cover catalog numbers are loaded in the Q2C system with pricing and lead times. Some catalog numbers will have minimum quantity restrictions.
Available catalog numbers of QO cover painted white are:
QOC16UFW
QOC16USW
QOC20UFWGW
QOC24UFW
QOC30UFW
QOC30UFWGW
QOC32UFW
QOC32U125CW (Used on Canadian Load Centres)
QOC40UFW
QOC42UFW



CTA-ID : 2032034
Was this helpful?
What can we do to improve the information ?