Technical FAQs

Ask a Question

<br />Customer asks if the CLS1 Crane hoist overtravel limit switch is still available?

Customer was advised that the Digest 170 page 17-16 shows the 9007-CLS1 and, yes, it is still available. Information can also be found on page 485 of 9006CT0101

CTA-ID : 2031962
Was this helpful?
What can we do to improve the information ?