Technical FAQs

Ask a Question

Will the LA4DC1U work with the new CAD32BD relay?

Issue:
Will the LA4DC1U work on the CAd32BD relay

Product Line:
IEC relays and accessories

Environment:
Products sold and used in the United States

Cause:
Identifying product compatibility

Resolution:
The CAD32BD with DC coil has built-in coil suppression protection as standard so the LA4DC1U is not needed.


CTA-ID : 2031917
Was this helpful?
What can we do to improve the information ?