Technical FAQs

Ask a Question

Customer asks if Class 8941 Duplex Motor Controllers are UL listed?

The components are UL Listed, however, the 8941 as a complete unit is not UL listed unless it is ordered with Form Y1.

CTA-ID : 2031987
Was this helpful?
What can we do to improve the information ?