Technical FAQs

Ask a Question

Can I field install a control power transformer to a 8536SD, Size 2 enclosed starter in standard enclosure?

There`s not enough room in the enclosure for the field addition of a CPT. Order a 9991 oversized enclosure, take the starter out of its present enclosure, install it in the new one, and then you can add a CPT. Also, use the 9070 type T CPT with separate mounted fuse blocks.

CTA-ID : 2031965
Was this helpful?
What can we do to improve the information ?