Technical FAQs

Ask a Question

Is a busway section AP2308G10 able to be connected to an AP2308G10ST? Will they fit together?

Issue:
Is a busway section AP2308G10 able to be connected to an AP2308G10ST?  Will they fit together?  

Product Line:
Busway.

Environment:
Products sold in the United States.

Cause:
Product features.

Resolution:
Yes, these two busway sections are compatible with each other, they will fit together.


CTA-ID : 2031809
Was this helpful?
What can we do to improve the information ?