Technical FAQs

Ask a Question

What type of lugs does circuit breaker catalog number JDP36250 use? What is the wrench size and the torque value?

The wire binding lugs use an allen head fastener size 5/16``. Torque the lugs to 225 inch pounds, or 18.75 foot pounds.

CTA-ID : 2031891
Was this helpful?
What can we do to improve the information ?