Technical FAQs

Ask a Question

What is the wire range of the lugs on a circuit breaker catalog number QO2150?

The wire range is (1) #1-300 kcmil aluminum or copper. Note also that this breaker takes up four spaces, and can be used in a single phase panel only.


CTA-ID : 2031880
Was this helpful?
What can we do to improve the information ?