Technical FAQs

Ask a Question

Is the ground fault function on the QO250GFI ground fault breakers rated at 30 milliamps?

No. The QO250GFI ground fault function is rated at 6 milliamps. A QO250EPD equipment protection device (EPD) breaker is rated at 30 milliamps.


CTA-ID : 2031871
Was this helpful?
What can we do to improve the information ?