Technical FAQs

Ask a Question

Can the operating handle of a H60XFA circuit breaker enclosure be padlocked in the ON position? <br /> <br />

This device can only be locked in the OFF position. A factory special to provide a lock-ON feature is not available.

CTA-ID : 2031887
Was this helpful?
What can we do to improve the information ?