Technical FAQs

Ask a Question

Does the QOUMF1 come with one mounting foot or two, one for line and load?

Issue:
Product Design Features

Product Line:
QOU Circuit breakers

Environment:
QOU accessories

Cause:
Ordering

Resolution:
The QOUMF1 is ONLY one mounting foot, would need to order 2 of them to have one for the line and one for the load.


CTA-ID : 2031863
Was this helpful?
What can we do to improve the information ?