Technical FAQs

Ask a Question

What is a LHF36300?

LHF has no lugs and has bus bar connections. It is a LHL breaker with lugs removed. If lugs are removed in the field the breaker must be secured with pan-mounting screws, or ``P`` screws (cover screws and nuts) installed securing the base to the cover.


CTA-ID : 2031735
Was this helpful?
What can we do to improve the information ?