Technical FAQs

Ask a Question

Is there a way to test ground fault on a Powerpact R frame breaker and not trip the breaker?

No. Primary injection, use of the Full Function Test Kit, and GF test button on the front of the trip unit will all trip the breaker.


CTA-ID : 2031733
Was this helpful?
What can we do to improve the information ?