Technical FAQs

Ask a Question

Can a HOM250GFI be used on a 240 V 2-wire circuit.<br />

The HOM-GFI requires a 120/240 V circuit. As long as there is no more than 240 V line to line and between 100 and 120 V line to ground it will work.
Since there is no load neutral conductor, leave the load neutral connection on the breaker empty. The pigtail must be connected to the grounded panel neutral.

CTA-ID : 2031765
Was this helpful?
What can we do to improve the information ?