Technical FAQs

Ask a Question

Why is the replacement bulb for 9999SP12R rated 6Vac?

The pilot light kit is powered by an thin wafer looking induction coil, which, when installed into the starter power plant, induces approximately 6VAC to power the light. It makes no difference what the operating voltage of the coil is because the induced voltage will always be the same. The magnetic lines of flux around the coil core induces the voltage onto the pilot light induction coil.


CTA-ID : 2031788
Was this helpful?
What can we do to improve the information ?