Technical FAQs

Ask a Question

What is the voltage rating of a QO115GFI ?

It is 120vac to ground. Can be applied on a 120/240 Vac single phase system.


CTA-ID : 2031756
Was this helpful?
What can we do to improve the information ?